This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
WiiFi support is newly added to TI Android DevKit. Extensive performance analysis is not yet done.
Do you see packet loss only with android or in linux too?
I suggest that you try this with linux too. This would help isolate if this is a driver issue or android issue.
We found that having a combined SDIO and wifi driver resulted in a better system stability in android on our evm. But as mentioned previously, we have not yet done any extensive testing.
We would recommend that you first verify wifi operation and performance on linux before moving to android.
Sample linux filesystem is available with the Linux PSP package. You can use that as your starting point.
Now I modified the following:
1. Loaded new F/W (349) and Driver (149).
2. Set the following param in tiwlan.ini
dot11PowerMode = 1, defaultPowerLevel = 1, PowerSavePowerLevel = 1
and tried. But no improvement. Do you want me to do any other specific test? I will try with Linux Image and update.For wifi-specific queries please use the WLAN Applications E2E forum http://e2e.ti.com/support/low_power_rf/f/307.aspx
We can only help with android integration.