This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

why disable drift guard property for dpll in BSP version A8 01 01

 Hi, all

I compare the source code between bsp A8010100 and A8010000, find that in bsp A8010100, disabled the drift guard property (    dpllInfo.driftGuardEnabled = FALSE). Could someone tell me the reason? Thank you!~

  • Hellen

    The driftguard is needed only when you have an end product that is exposed to large varying temperature and/or voltage. When this flag is enabled, DPLL can do auto-recalibration whenever it detects drifts in temp/volt. While this re-calibration is in progress, if care is not taken to stall the accesses to the modules affected by this re-calibrating DPLL, it could lead to system instability. So unless you are designing a product that will be used in such extreme conditions, it is recommended to disable driftguard flag for the DPLLs.

    -Madhvi