Other Parts Discussed in Thread: UNIFLASH,
Dear experts,
When I tested with UNIFLASH 6.1.0 on Ubuntu 18.04 host with TDA4VM EVM, I got segment fault. Is there a known issue?
I tested Windows UNIFLASH 6.1.0 it works fine. I tried minicom and got "CCCCC" in the serial port.
~/ti/uniflash_6.0.0$ ./dslite.sh --mode processors -c /dev/ttyUSB1 -f ./processors/FlashWriter/j721e_evm/uart_j721e_evm_flash_programmer_release.tiimage -i 0 Executing the following command: > ./ProcessorSDKSerialFlash -c /dev/ttyUSB1 -f ./processors/FlashWriter/j721e_evm/uart_j721e_evm_flash_programmer_release.tiimage -i 0 For more details and examples, please refer to the UniFlash Quick Start guide. ---------------------------------------------------------------------------- ProcessorSDKSerialFlash CLI Tool Copyright (C) 2017-2019 Texas Instruments Incorporated - http://www.ti.com/ Version 1.2.0.0 ---------------------------------------------------------------------------- Downloading Flash Programmer.. Enabling SysFw transfer!!! Opening Port Successful! ./dslite.sh: line 75: 26184 Segmentation fault (core dumped) ./ProcessorSDKSerialFlash -c /dev/ttyUSB1 -f ./processors/FlashWriter/j721e_evm/uart_j721e_evm_flash_programmer_release.tiimage -i 0