Hi,
what is the temp range of TMSDC6726BRFPA225?
In the DS it indicates that with an A it is -40 to 105.
Further down in the DS it says 0 to 90.
Thanks
Fred
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
what is the temp range of TMSDC6726BRFPA225?
In the DS it indicates that with an A it is -40 to 105.
Further down in the DS it says 0 to 90.
Thanks
Fred
Fred,
Thanks for reposting the pictures. Yes, I saw the same thing and agree it is confusing. Let me work with the documentation team to confirm which is true and come back to you.
Fred
In this case, there is a typo in the Package option addendum.
There are clues here.
1. The part number is for a -40C to 105C part. If it were the lower temp range then it would not have the "A" between RFP and 225.
2. The same package is used for the TMSDC6722BRFPA225 and it shows the correct temp range.
I'll work on getting this corrected.
--Paul