Hi all,
Based on DM368 and supported dvsdk_2_10_01_18(H264 codec version is 02.00.00.09),
I set codec parameter encQuality=2 to use Platinum mode,
frame rate is about 19 FPS, but incorrect compressed result were created as below,
so I tried to switch to lower mode setting(encQuality=0),
the compressed frames are correct, but the frame rate is dropped to about 13 FPS.
all of h264 parms. set-up are here 5126.parms.txt
so how to meet the requirement of correct 3M@20FPS H264 encode?
Any comments will be appreciated!!
thanks.
Charles