Part Number: TDA4VM
Other Parts Discussed in Thread: OMAPL138
HI
i need to create a config file for kernel 5.4.82. I down load the ti tools from the git site. followed the script but it only generated j7_pcie_rc defconfig. I need to get the
tisdk_j7-evm_defconfig
to build the kernel version 5.4.82.
Any suggestions please let me know. I wonder if i can use the config file from sdk 7.1.00.10 which is based on kernel 5.4.74. Any help as to how to create the config would be great. I need the kernel 5.4.82 because of some fixes that was made.
i run the option to list what i can get the config and got the below which does not include tisdk_j7-evm_defconfig
The following are a list of buildable defconfigs:
1. ti_sdk_am3x_release
2. ti_sdk_am4x_release
3. ti_sdk_dra7x_release
4. ti_sdk_omap2_release
5. ti_sdk_k2g_release
6. ti_sdk_keystone_release
7. ti_sdk_omapl138_release
8. ti_sdk_am3x_debug
9. ti_sdk_am4x_debug
10. ti_sdk_dra7x_debug
11. ti_sdk_omap2_debug
12. ti_sdk_k2g_debug
13. ti_sdk_keystone_debug
14. ti_sdk_omapl138_debug
15. ti_sdk_arm64_release
16. ti_sdk_arm64_debug
17. am3_eth_module
18. am4_eth_module
19. dra7_eth_module
20. k2_eth_module
21. am3_can_built_in
22. am3_mmc_module
23. am4_mmc_module
24. k2_mmc_module
25. omapl138_mmc_module
26. dra7_mmc_module
27. am3_pio_musb
28. am6_eth_module
29. am6_mmc_module
30. j7_pcie_rc
Thanks