Other Parts Discussed in Thread: AM5749
On a Windows Xeon Box in Windows 10 building image THE processing demo found here for the AM5749 IDK ...
Following instructions verbatim, the build errors-out with the cause being:
Invoking: XDCtools"C:/ti/xdctools_3_55_02_22_core/xs" --xdcpath="C:/ti/bios_6_76_03_01/packages;C:/ti/pdk_am57xx_1_0_17/packages;C:/ti/ndk_3_61_01_01/packages;C:/ti/ipc_3_50_04_08/packages;C:/ti/uia_2_30_01_02/packages;../../../../evmam572x/platform;" xdc.tools.configuro -o configPkg -t gnu.targets.arm.A15F -p evmAM572x_mcip_host -r debug -c "C:/ti//gcc-arm-none-eabi-7-2018-q2-update" "../image_processing_evmam572x_host.cfg"
making package.mak (because of package.bld) ...
generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
configuring image_processing_evmam572x_host.xa15fg from package/cfg/image_processing_evmam572x_host_pa15fg.cfg ...
js: "C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/image_processing/ipc/evmam572x/host/no_instrumentation/image_processing_evmam572x_host.cfg", line 154: xdc.services.global.XDCException: xdc.PACKAGE_NOT_FOUND: C:\ti\ipc_3_50_04_08\packages\ti\sdo\ipc\interfaces\package.xdc found along the package path, but no schema file was found. Ensure that the package 'ti.sdo.ipc.interfaces' is completely built.
"./package/cfg/image_processing_evmam572x_host_pa15fg.cfg", line 196
gmake.exe: *** [package.mak:218: package/cfg/image_processing_evmam572x_host_pa15fg.xdl] Error 1
js: "C:/ti/xdctools_3_55_02_22_core/packages/xdc/tools/Cmdr.xs", line 52: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake[2]: *** [makefile:151: configPkg/linker.cmd] Error 1
gmake[2]: Leaving directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/image_processing/ipc/evmam572x/host/no_instrumentation/build'
gmake[1]: *** [makefile:75: am57xx_demo] Error 2
gmake[1]: Leaving directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/image_processing/ipc/evmam572x'
gmake: *** [makefile:147: imageproc_demo] Error 2
1) Is a schema is missing?
2) Where can I get (or how can I generate) the missing schema?
3) Where should I place it once I have it?
Complete output follows in file attachment:
*************************************************** Environment Configuration: *************************************************** SDK_INSTALL_PATH : C:/ti PDK_INSTALL_PATH : C:/ti/pdk_am57xx_1_0_17/packages GMAKE_INSTALL_PATH : C:/ti/xdctools_3_55_02_22_core PDK_SOC : am57xx PDK_VERSION : 1_0_17 RULES_MAKE : C:/ti/pdk_am57xx_1_0_17/packages/ti/build/Rules.make *************************************************** IPC_PLATFORM: DRA7XX IPC_ALT_PLATFORM: AM572X AM571X PROC_SDK_INSTALL_PATH : C:/ti/processor_sdk_rtos_am57xx_6_03_00_106 ************************************************************************** Changing to short name to support directory names containing spaces current directory: C:/ti/processor_sdk_rtos_am57xx_6_03_00_106 PROCESSOR SDK BUILD ENVIRONMENT CONFIGURED ************************************************************************** C:\ti\processor_sdk_rtos_am57xx_6_03_00_106>make demo_clean 'make' is not recognized as an internal or external command, operable program or batch file. C:\ti\processor_sdk_rtos_am57xx_6_03_00_106>gmake demo_clean C:/ti/xdctools_3_55_02_22_core/gmake -C ./demos/image_processing/ipc/evmam572x clean gmake[1]: Entering directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/image_processing/ipc/evmam572x' C:/ti/xdctools_3_55_02_22_core/gmake -C ./host/no_instrumentation/build clean gmake[2]: Entering directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/image_processing/ipc/evmam572x/host/no_instrumentation/build' rm -f "image_processing_evmam572x_host.out" "configPkg\linker.cmd" "configPkg\compiler.opt" "image_processing_evmam572x_host.hex" rm -r -f "configPkg" rm -f "mcip_bmp_utils.d" "mcip_master_main.d" "mcip_process.d" "mcip_webpage.d" "mcip_webpage_utils.d" "nimu_osal.d" rm -f "mcip_bmp_utils.o" "mcip_master_main.o" "mcip_process.o" "mcip_webpage.o" "mcip_webpage_utils.o" "nimu_osal.o" Finished clean gmake[2]: Leaving directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/image_processing/ipc/evmam572x/host/no_instrumentation/build' C:/ti/xdctools_3_55_02_22_core/gmake -C ./dsp1/no_instrumentation/build clean gmake[2]: Entering directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/image_processing/ipc/evmam572x/dsp1/no_instrumentation/build' rm -f "image_processing_evmam572x_dsp1.out" "configPkg\linker.cmd" "configPkg\compiler.opt" "image_processing_evmam572x_dsp1.hex" rm -r -f "configPkg" rm -f "mcip_core.d" "mcip_core_task.d" "mcip_slave_main.d" rm -f "mcip_core.obj" "mcip_core_task.obj" "mcip_slave_main.obj" Finished clean gmake[2]: Leaving directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/image_processing/ipc/evmam572x/dsp1/no_instrumentation/build' C:/ti/xdctools_3_55_02_22_core/gmake -C ./dsp2/no_instrumentation/build clean gmake[2]: Entering directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/image_processing/ipc/evmam572x/dsp2/no_instrumentation/build' rm -f "image_processing_evmam572x_dsp2.out" "configPkg\linker.cmd" "configPkg\compiler.opt" "image_processing_evmam572x_dsp2.hex" rm -r -f "configPkg" rm -f "mcip_core.d" "mcip_core_task.d" "mcip_slave_main.d" rm -f "mcip_core.obj" "mcip_core_task.obj" "mcip_slave_main.obj" Finished clean gmake[2]: Leaving directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/image_processing/ipc/evmam572x/dsp2/no_instrumentation/build' gmake[1]: Leaving directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/image_processing/ipc/evmam572x' C:/ti/xdctools_3_55_02_22_core/gmake -C ./demos/bigdataipc clean \ PLATFORM=DRA7XX \ XDC_INSTALL_DIR="C:/ti/xdctools_3_55_02_22_core" gmake[1]: Entering directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/bigdataipc' # # Cleaning host_bios examples... C:/ti/xdctools_3_55_02_22_core/gmake -C host_bios/simple_buffer_example clean gmake[2]: Entering directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/bigdataipc/host_bios/simple_buffer_example' C:/ti/xdctools_3_55_02_22_core/gmake -C host clean gmake[3]: Entering directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/bigdataipc/host_bios/simple_buffer_example/host' C:/ti/xdctools_3_55_02_22_core/bin/rm -rf bin gmake[3]: Leaving directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/bigdataipc/host_bios/simple_buffer_example/host' C:/ti/xdctools_3_55_02_22_core/gmake -C dsp clean gmake[3]: Entering directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/bigdataipc/host_bios/simple_buffer_example/dsp' C:/ti/xdctools_3_55_02_22_core/bin/rm -rf bin gmake[3]: Leaving directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/bigdataipc/host_bios/simple_buffer_example/dsp' C:/ti/xdctools_3_55_02_22_core/bin/rm -rf install gmake[2]: Leaving directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/bigdataipc/host_bios/simple_buffer_example' # # Cleaning host_linux examples... C:/ti/xdctools_3_55_02_22_core/gmake -C host_linux/simple_buffer_example clean gmake[2]: Entering directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/bigdataipc/host_linux/simple_buffer_example' C:/ti/xdctools_3_55_02_22_core/gmake -C host clean gmake[3]: Entering directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/bigdataipc/host_linux/simple_buffer_example/host' C:/ti/xdctools_3_55_02_22_core/bin/rm -rf bin gmake[3]: Leaving directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/bigdataipc/host_linux/simple_buffer_example/host' C:/ti/xdctools_3_55_02_22_core/gmake -C dsp clean gmake[3]: Entering directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/bigdataipc/host_linux/simple_buffer_example/dsp' C:/ti/xdctools_3_55_02_22_core/bin/rm -rf bin gmake[3]: Leaving directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/bigdataipc/host_linux/simple_buffer_example/dsp' C:/ti/xdctools_3_55_02_22_core/bin/rm -rf install gmake[2]: Leaving directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/bigdataipc/host_linux/simple_buffer_example' gmake[1]: Leaving directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/bigdataipc' C:/ti/xdctools_3_55_02_22_core/bin/rm -rf ./demos/posix-smp/bin C:\ti\processor_sdk_rtos_am57xx_6_03_00_106>gmake demo C:/ti/xdctools_3_55_02_22_core/gmake -C ./demos/image_processing/ipc/evmam572x all gmake[1]: Entering directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/image_processing/ipc/evmam572x' C:/ti/xdctools_3_55_02_22_core/gmake -C ./host/no_instrumentation/build all gmake[2]: Entering directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/image_processing/ipc/evmam572x/host/no_instrumentation/build' Building file: ../image_processing_evmam572x_host.cfg Invoking: XDCtools "C:/ti/xdctools_3_55_02_22_core/xs" --xdcpath="C:/ti/bios_6_76_03_01/packages;C:/ti/pdk_am57xx_1_0_17/packages;C:/ti/ndk_3_61_01_01/packages;C:/ti/ipc_3_50_04_08/packages;C:/ti/uia_2_30_01_02/packages;../../../../evmam572x/platform;" xdc.tools.configuro -o configPkg -t gnu.targets.arm.A15F -p evmAM572x_mcip_host -r debug -c "C:/ti//gcc-arm-none-eabi-7-2018-q2-update" "../image_processing_evmam572x_host.cfg" making package.mak (because of package.bld) ... generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ... configuring image_processing_evmam572x_host.xa15fg from package/cfg/image_processing_evmam572x_host_pa15fg.cfg ... js: "C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/image_processing/ipc/evmam572x/host/no_instrumentation/image_processing_evmam572x_host.cfg", line 154: xdc.services.global.XDCException: xdc.PACKAGE_NOT_FOUND: C:\ti\ipc_3_50_04_08\packages\ti\sdo\ipc\interfaces\package.xdc found along the package path, but no schema file was found. Ensure that the package 'ti.sdo.ipc.interfaces' is completely built. "./package/cfg/image_processing_evmam572x_host_pa15fg.cfg", line 196 gmake.exe: *** [package.mak:218: package/cfg/image_processing_evmam572x_host_pa15fg.xdl] Error 1 js: "C:/ti/xdctools_3_55_02_22_core/packages/xdc/tools/Cmdr.xs", line 52: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted. gmake[2]: *** [makefile:151: configPkg/linker.cmd] Error 1 gmake[2]: Leaving directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/image_processing/ipc/evmam572x/host/no_instrumentation/build' gmake[1]: *** [makefile:75: am57xx_demo] Error 2 gmake[1]: Leaving directory 'C:/ti/processor_sdk_rtos_am57xx_6_03_00_106/demos/image_processing/ipc/evmam572x' gmake: *** [makefile:147: imageproc_demo] Error 2