Part Number: TDA3XEVM
Hi,
I'm working on adding memory protection to the DSPs on a TDA3 and have some questions. I'm using PDK version 01.10.04.05.
I can successfully add protection to a memory area, using `DSPXMCSetMPAXSegment`, and verify that I get memory exceptions if I try to access the protected memory using either read or write with the corresponding access permission set.
However, after I am done using the memory I would like to remove the access permissions, so that everything "goes back to normal". Is this possible, and if so how can I do it?
So far I have tried with another call to `DSPXMCSetMPAXSegment` but with the size specified as `DSPXMC_SEGSZ_DISABLED` as I interpret it as it would disable that MPAX segment so that it no longer checks any accesses. I have also tried to setup another MPAX segment with a higher ID that should shadow any previous entries on any overlapping memory area. Neither of these approaches have been successful in my testing.
I get errors like
XMC Exception MPFAR=0x8df00fc0 MPFSR=0x110 Security violation, Local L1/L2 cache memory Fault Supervisor Write violation, Fault ID=0x0 [t=0x0006c0bd] ti.sysbios.family.c64p.Exception: ERROR: F ti.sysbios.family.c64p.Exception: line 265: E_exceptionMax: pc = 0x8400f6d8, sp = 0x858007f8. xdc.runtime.Error.raise: terminating execution
when I try to access the relevant memory after first setting restrictive access and then trying to remove it or setting a permissive access according to above.
Thanks in advance,
Love