Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Compiler crash

Part Number: TDA4VM

 

Sometime compiler crash with the following condition.

■Test Code

CompilerCrush.zip

CompilerCrush.zip 

■Procedure for reproducing problems

① Prepare the TDA4VM-EVM.

 

② Build with CCS10.

 

③ The following message appears and the build fails illegally.

 

ccs10_log.txt

**** Clean-only build of configuration Debug for project CompilerCrush ****

"C:\\ti\\ccs1011\\ccs\\utils\\bin\\gmake" -k -j 12 clean -O 
 
DEL /F  "CompilerCrush.out" 
DEL /F "main.obj" 
DEL /F "main.d" 
C:\Users\p212032\workspace_v10\CompilerCrush\Debug\CompilerCrush.out が見つかりませんでした。
C:\Users\p212032\workspace_v10\CompilerCrush\Debug\main.obj が見つかりませんでした。
Finished clean
 

**** Build Finished ****

**** Build of configuration Debug for project CompilerCrush ****

"C:\\ti\\ccs1011\\ccs\\utils\\bin\\gmake" -k -j 12 all -O 
 
Building file: "../main.cpp"
Invoking: C7000 Compiler
"C:/ti/ccs1011/ccs/tools/compiler/ti-cgt-c7000_1.4.1.LTS/bin/cl7x" -O3 --include_path="C:/Users/p212032/workspace_v10/CompilerCrush" --include_path="C:/ti/ccs1011/ccs/tools/compiler/ti-cgt-c7000_1.4.1.LTS/include" -g --diag_warning=225 --diag_wrap=off --display_error_number --preproc_with_compile --preproc_dependency="main.d_raw"  "../main.cpp"
 
>> Compilation failure
subdir_rules.mk:9: recipe for target 'main.obj' failed
 
>>>> Optimizer terminated abnormally
>>>>    in function main()
>>>>    in file "../main.cpp"
This is caused by a defect in the TI C/C++ Optimizer.
TI Customer Support may be able to suggest a workaround to avoid this.
 
Upgrading to the newest version of the compiler may fix this problem.
 
Contact TI in the E2E support forums at http://e2e.ti.com under
"Development Tools", "TI C/C++ Compiler".  See the link titled
"Submitting an issue".
 
We need to see this ENTIRE error message and a complete, reproducible
test case including ALL of the command-line options.
Include the .pp file created by option --preproc_with_comment
 
gmake: *** [main.obj] Error 1
gmake: Target 'all' not remade because of errors.

**** Build Finished ****
 

■Remarks

const uint64_t nSize = 0x100000000;

Occurs when exceeding the 32bit range

 

Does not occur when optimization is disabled

 

■Environments

PSDK:V07.01.00 

Thanks and Best regards,

HaTa.