Part Number: DRA829V
Hello TI team,
We have a use case for hardware accelerated video rotation on CSI Rx streaming output. First we were targeting VP Stream2 from CSI Rx to VPAC but section 6.10.4.1.4 in the TRM says that YUV input is not supported on VISS so it looks like a no go for us. Moreover there is no way mentioned for LDC to take input from SL2 memory of VPAC.
We're now targeting to use LDC in mem2mem mode to do a capture + mem2mem video pipeline; can you please provide your input on the following queries:
1. Can you confirm that LDC can't indeed be used on-the-fly by streaming input to VPAC?
2. Is such a use for VPAC LDC possible that we capture frames using CSI Rx into DDR, then pass those (linear) memory buffers to LDC for processing and eventually to our application (e.g. storage) so we get rotation on the captured frames.
3. If no. 2 is the intended way to use LDC in real time then how can we match data rate between CSI Rx output and LDC processing for streaming use-case?
Best regards