MP3 encode version : mp3_3_5_00_production
SDK version : dvsdk3_10_00_19
CPU : DM368
test AP : dvsdk3_10_00_19/dvsdk_demo_3_10_00_16
enable audio code engine and ipmrement mp3 encode codec in to encode AP.
When run the encode ap and only encode audio , the cpu loading average in 80%
This is my command :
#./encode -a /mnt/tmp/1.mp3
And when i review the encode file , one channel is nosie , one channel is not right 1KHz waveform.
What do i need to check ?