Other Parts Discussed in Thread: OMAP-L137
Hello,
where can i find a gel file for my C6745 chip?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAP-L137
Hello,
where can i find a gel file for my C6745 chip?
Hi,
You can get GEL file of DSK C6747 from the link given below.
DSP GEL file.
http://support.spectrumdigital.com/boards/evmomapl137/revg/
As C6747 DSK can also be used as C6745 DSK as they are similar. So, GEL file for C6747 DSK should work with C6745 as well but one needs to take care of the peripheral settings as they differ slightly in peripherals. I am not sure of those settings.
For your information, you will also find ARM GEL file in the link mentioned above, that GEL file is for OMAP-L137. It is because OMAP-L137 and C6747 has the same starter kit but their GEL files are different.
Hope this helps.
Best Regards,
Ankit Agrawal
Thanks a lot. I can use the GEL file from spectrum digital.
Are there any code examples for my DSP?
You can download ZIP file mentioned below.
----------------------------------------
EVMOMAPL137 Test Code
EVMOMAPL137 test code and board support library
----------------------------------------
from the link given below.
http://support.spectrumdigital.com/boards/evmomapl137/revg/
But these are examples code for C6747 DSK. For C6745 DSK, you may need to make some changes as per C6745 specifications as there are some differences.
Hope this helps.
Best Regards,
Ankit Agrawal