This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to use a generated TI library in a CCS project??

I got a audio codec library from TI. I included one of the libraries in my CCS project.

Then I called one of the functions of the included library from my application.

It is keeping on asking to add the header files and the source files and it is not getting compiled.

Can someone suggest a solution for this????

  • Once you include the library and include the header files then there should not be any problem. Header file should be included in the file from where you are calling the functions of library.

     

    In CCS4 when you are including the library through project options, please check that path of library is correct or not? 

  • I tried to include the library from the attached folder. Then I called a function which is in the header file of that library.

    when i was trying to compile it is not happening. Errors and warnings are keeping on coming for header files and source files for inclusion.

    Can some one try out doing this or suggest any way for porting that???

    tgu.zip