Part Number: AM5749
Other Parts Discussed in Thread: ADS8422, ADC3660,
Hi,
I'm currently developping the interface between the GPMC parrelle port and an ADC (ADS8422). To fit with ADC requirement, I need to set the RdAccessTime and PageBurstAccessTime parameter properly. The related time (in ns) is calculated according to a number of GPMC_FCLK cycles. But the maximum cycles of each of them do not fit with what is expexted due to the base frequency of 266MHz.
For example, the maximum cycle number of RdAccessTime is '31'. At 266MHz, the cycle delay is 3.75ns, so 31 cycles is 116.5ns. The requiered delay should be more than 550ns.
Is it possible to reduce the GPMC_FCLK from 266MHz to 50MHz? is there any prescaler into the GPMC clock domain?
Best Regards,
Sylvain