This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5402 Booting

Struggling to boot C5402 using parallel EEPROM boot mode. I have two questions.

 

1.                          The document SPRA618B section 2.2.3 shows that the bootloader gets the source address from either I/O port 0FFFFh or data memory address 0FFFFh.  

If I use the data memory, what address in EEPROM should I locate the start address of boot table?

 

2.                          I’m also trying to boot C5402 on DSK using EEPROM on DSK board. Document SPRA773 section 5.4 indicates that Flashburn is available for CCS2. I couldn’t get it using CCS update advisor. Could you get it for me? Or, should I update the version of CCS? Currently, I’m using CCS DSK ver.2.1.