Hello everyone,
I’m a little confused about the specification for mDDR memory which can be used with the C674x DSPs. According to the datasheet for the C6746, one must use a -400 speed-grade part (see section 6.11.3.2). However, the maximum clock speed allowed is 133MHz for mDDR, suggesting an LPDDR266 part or better is all that is really required.
Looking at the OMAP-L138/TMS320C6748 EVM from LogicPD, they’re using an mDDR/LPDDR chip which has a data rate of “LPDDR333”. Thus I assume the -400 requirement only applies to DDR2, and not to mDDR. Can you please confirm that an LPDDR333 memory is suitable? We had hoped to use a LPDDR333 part.
Thanks,
Mike