This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3530 USB Download Error

Other Parts Discussed in Thread: OMAP3530

Hi,all:

         I have a based OMAP3530 development board. I want to download X-loader and U-boot via USB. The operation and settings are as below.

          (1) software :  Flash v1.4

                        choose target:  Custom OMAP35xx Board

                        select target connection type :   USB

                        choose the target memory type: NAND

                        select memory options:  default

                         choose operate parameter : download

                         address: 0x00000000

         (2)  Based OMAP3530 development board  boot from USB.

         But the Flash v1.4 prompts:

-stdout

-omap 3

-t 60

-p CUSTOM_OMAP35XX_BOARD

-2

chip_erase NANDINFO 0

Leaving parameter file:temp_script.txt

@temp_script.txt

Looking for device (omap usb)

Please turn on device

Waiting for device (omap usb)

Cannot open device

Console program failed, exit code: 2