Part Number: TMS320C6748
Other Parts Discussed in Thread: OMAP-L138
Dea all,
We are developing a new board based on TMS320C6748 chip. The new board is pretty similar to the LCDK6748 eval kit, but DDR chip memory (W971GG6KB-25, U17 on the Eval schematics) and NAND Flash (MT29F4G16ABADAH4:D, U18 on the Eval kit) had been replaced (DDR SDRAM due basically had been obsoleted). They have been replaced by W971GG6SB-25 (DDR2 SDRAM 1Gb) and MT29F2G16ABAEAWP-AIT(2Gb NAND Flash).
As the size of the DDR2 SDRAM is the same as in the EVAL Kit (1Gb), I think minor changes or update for this will be needed. Do you agree with this? If not what should I need to do?
However size of the NAND Flash is now 2Gb, when in Eval kit is 4Gb.
I have been looking in the GEL file (..ccs\ccs_base\emulation\boards\lcdkc6748\gel\C6748_LCDK.gel) where to update the size of the NAND Flash and searching on the documentation available (including forum) but I dont see where I should update the size.
Please, would you be so kind to explain me, what do I need update for the new board? Which files? Any documentation of this?
Thanks in advance,
Joaquin.