This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About the error when the DSP Bridge MPEG4 encode is executed

Hello.
I am [urabe].
The DSP program development is done based on the sample code of DSPBridge (TI offer) now.
Then, please teach causing though it is a situation that cannot be executed because of the following errors.

The system requirements
BaseImage: Module DLLFile:m4venc_sn.dll64P that our company made based on sample child code
     mp4vdec_sn.dll64P
     usn.dll64P
    
The following errors occur when the encode processing is executed from ARM in the above-mentioned.

node_create: failed to load create code: 0xffffffac

****************LCML ERROR : DSP ************************
Error: Create the Node : Err Num = ffffffac
****************LCML ERROR : DSP ************************


This concludes my report.