Part Number: TDA4VM
Hi,
In Processor SDK 7.02, TI has enabled TFlite-runtime support. Can a node inside an openVX graph call the delegate function, which will dispatch subgraphs to A72 or TIDL ?
regards,
Victor
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
Hi,
In Processor SDK 7.02, TI has enabled TFlite-runtime support. Can a node inside an openVX graph call the delegate function, which will dispatch subgraphs to A72 or TIDL ?
regards,
Victor
Hi Victor,
As TFLite sets up OpenVx sub-graphs in the delegate functions, its unlikely that this can be wrapped in an OpenVx node and connect it to another graph running on A72.
Regards,
Shyam
Hi Shyam,
Thanks for the useful information.
Is it possible to connect a camera capture node and display node to an openVX graph generated by TF-lite ?
regards,
Victor
Hi Victor,
Yes this should be possible,
You can split your application into 3 parts,
1. OpenVx graph1 - CSI-Rx -> VISS -> LDC -> MSC -> Pre-Processing (Get output in RGB/BGR planar data)
2. Use DLR RT or TFLite RT
3. OpenVx graph 2 - Post-processing -> Mosaic Node (if required) -> DSS
Note at the boundaries of DLR-RT, currently it might require a copy back and forth. But it should be possible to avoid this if all buffers are allocated in DDR_SHARED_MEM and there is a way to tell the DLR-RT.
Regards,
Shyam