Other Parts Discussed in Thread: DM3730
Hi all:
we use most recently DSP SDK(DVSDK4.01.00.09) run on EVK , the engineer report the prebuild not work with DM3730 EVK ,dose any one have had a test with this file?
other question is when we use source code rebuild , the system run good and can play all of test media with DVI port ,but only can play all of test media on DVI port , when we switch display port to LCD , it only can play low resolution media , it will prompt "DISPC err:VID1_FIFO_UNDERFLOW" , our OS is android 2.2 , please help .
Thanks!
Rex