This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Change single_camera usecase

Part Number: TDA4VM

Now we have some TDA4VM/J721EX boards and "psdk_rtos_auto_j7_06_02_00_21" sdk.

I can run single_camera usecase well with the config RIN0 and MIPI CSI0_D0.

How can i change the config to RIN1 and MIPI CSI0_D1?