Part Number: TMS320C6657
Hello
I am using external clock mode in TMS320C6657 timer. The clock input on TINPL pin is 10K in frequency, and I would like to generate a timer event, such as TINT2L, in same frequency.
In this case, how to setup the timer period? when I set PRDLO to 1, the TINT2L is generated in 5K frequency. While, when I set PRDLO to 0, no TINT2L timer interrupt is generated.
How to create the same frequency interrupt as that on the TINPL input? Thanks!