This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2P-ACD: TDA2SX: OOM happened when rendering

Part Number: TDA2P-ACD

hi 

oom-killer is invoked when we are rendering our texture, log as below:

[ 160.684791] 3dRender invoked oom-killer: gfp_mask=0x24000c4, order=0, oom_score_adj=0
[ 160.684804] 3dRender cpuset=/ mems_allowed=0
[ 160.684827] CPU: 1 PID: 561 Comm: 3dRender Tainted: G W O 4.4.84 #1
[ 160.684836] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 160.684844] Backtrace:
[ 160.684869] [<c00131d4>] (dump_backtrace) from [<c00133d0>] (show_stack+0x18/0x1c)
[ 160.684876] r7:ee1b9078 r6:60080013 r5:00000000 r4:c078a7d0
[ 160.684906] [<c00133b8>] (show_stack) from [<c023b0e8>] (dump_stack+0x8c/0xa0)
[ 160.684922] [<c023b05c>] (dump_stack) from [<c0121aa0>] (dump_header+0x5c/0x1ac)
[ 160.684929] r7:ee1b9078 r6:00000000 r5:d8051b34 r4:ee1b8c00
[ 160.684954] [<c0121a44>] (dump_header) from [<c00d5738>] (oom_kill_process+0x2fc/0x448)
[ 160.684962] r10:c07737b8 r9:0000b67c r8:00000137 r7:ee1b9078 r6:000249fc r5:d8051b34
[ 160.684984] r4:ee1b8c00
[ 160.684996] [<c00d543c>] (oom_kill_process) from [<c00d5be4>] (out_of_memory+0x2f0/0x32c)
[ 160.685003] r10:c07737b8 r9:0000b67c r8:c07737b8 r7:c0773a38 r6:000249fc r5:d8051b34
[ 160.685024] r4:ee1b8c00
[ 160.685037] [<c00d58f4>] (out_of_memory) from [<c00daaac>] (__alloc_pages_nodemask+0x924/0x964)
[ 160.685044] r10:c07ab600 r9:024000c4 r8:00000000 r7:c077066c r6:d8050000 r5:00000000
[ 160.685070] r4:00000000
[ 160.685147] [<c00da188>] (__alloc_pages_nodemask) from [<bf0052e4>] (NewAllocPagesLinuxMemArea+0xcc/0x278 [pvrsrvkm])
[ 160.685154] r10:00004000 r9:00000000 r8:00000000 r7:bf033c6c r6:00000118 r5:00000046
[ 160.685174] r4:ef4acd18
[ 160.685284] [<bf005218>] (NewAllocPagesLinuxMemArea [pvrsrvkm]) from [<bf00089c>] (OSAllocPages_Impl+0xe4/0xfc [pvrsrvkm])
[ 160.685291] r10:00000000 r9:d8033e00 r8:0005a000 r7:82014200 r6:d8051ca0 r5:80000203
[ 160.685310] r4:82014200
[ 160.685420] [<bf0007b8>] (OSAllocPages_Impl [pvrsrvkm]) from [<bf008214>] (BM_ImportMemory+0x284/0x580 [pvrsrvkm])
[ 160.685427] r5:80000203 r4:ec619b80
[ 160.685544] [<bf007f90>] (BM_ImportMemory [pvrsrvkm]) from [<bf0088bc>] (BM_Alloc+0x3ac/0x50c [pvrsrvkm])
[ 160.685550] r10:00000040 r9:ee152d00 r8:0005a000 r7:ed5fc908 r6:ee6c3100 r5:ec619b80
[ 160.685571] r4:80000203
[ 160.685685] [<bf008510>] (BM_Alloc [pvrsrvkm]) from [<bf008c38>] (AllocDeviceMem+0xb4/0x194 [pvrsrvkm])
[ 160.685692] r10:bf03320c r9:ec619b80 r8:00000000 r7:80000003 r6:d8051d4c r5:ed5fc900
[ 160.685713] r4:00000000
[ 160.685830] [<bf008b84>] (AllocDeviceMem [pvrsrvkm]) from [<bf0095e0>] (_PVRSRVAllocDeviceMemKM+0xb8/0x224 [pvrsrvkm])
[ 160.685836] r9:ee22a6c0 r8:f18d9000 r7:d80339c0 r6:eeae2700 r5:ec619b80 r4:80000003
[ 160.685964] [<bf009528>] (_PVRSRVAllocDeviceMemKM [pvrsrvkm]) from [<bf014f44>] (PVRSRVAllocDeviceMemBW+0x194/0x40c [pvrsrvkm])
[ 160.685971] r7:d80339c0 r6:00000000 r5:f18da000 r4:00000000
[ 160.686094] [<bf014db0>] (PVRSRVAllocDeviceMemBW [pvrsrvkm]) from [<bf017ac4>] (BridgedDispatchKM+0x94/0x25c [pvrsrvkm])
[ 160.686101] r8:f18da000 r7:f18d9000 r6:bf014db0 r5:d80339c0 r4:d8051e68
[ 160.686225] [<bf017a30>] (BridgedDispatchKM [pvrsrvkm]) from [<bf00465c>] (PVRSRV_BridgeDispatchKM+0x180/0x338 [pvrsrvkm])
[ 160.686232] r8:00000040 r7:ee22a6c0 r6:000000bb r5:c01c6707 r4:d8051e68
[ 160.686311] [<bf0044dc>] (PVRSRV_BridgeDispatchKM [pvrsrvkm]) from [<c02e4a90>] (drm_ioctl+0x140/0x454)
[ 160.686317] r7:eebb3000 r6:c07e3690 r5:0000001c r4:d8051e68
[ 160.686342] [<c02e4950>] (drm_ioctl) from [<c0135314>] (do_vfs_ioctl+0x3f0/0x614)
[ 160.686348] r10:00000000 r9:d8050000 r8:723da564 r7:00000081 r6:ee22a840 r5:eea69d40
[ 160.686369] r4:723da564
[ 160.686382] [<c0134f24>] (do_vfs_ioctl) from [<c0135574>] (SyS_ioctl+0x3c/0x64)
[ 160.686388] r10:00000000 r9:d8050000 r8:723da564 r7:401c6440 r6:ee22a840 r5:00000081
[ 160.686408] r4:ee22a841
[ 160.686422] [<c0135538>] (SyS_ioctl) from [<c000fae0>] (ret_fast_syscall+0x0/0x34)
[ 160.686429] r9:d8050000 r8:c000fc84 r7:00000036 r6:401c6440 r5:723da564 r4:0000001c
[ 160.686484] Mem-Info:
[ 160.686502] active_anon:25119 inactive_anon:1618 isolated_anon:0
[ 160.686502] active_file:2078 inactive_file:7891 isolated_file:0
[ 160.686502] unevictable:0 dirty:0 writeback:0 unstable:0
[ 160.686502] slab_reclaimable:1011 slab_unreclaimable:3355
[ 160.686502] mapped:43027 shmem:1667 pagetables:1216 bounce:0
[ 160.686502] free:63930 free_pcp:57 free_cma:41949
[ 160.686530] DMA free:105352kB min:1604kB low:2004kB high:2404kB active_anon:41332kB inactive_anon:2320kB active_file:280kB inactive_file:12kB unevictable:0kB isolated(anon):0kB isolated(file):0kB present:753664kB managed:342000kB mlocked:0kB dirty:0kB writeback:0kB mapped:141656kB shmem:2340kB slab_reclaimable:4044kB slab_unreclaimable:13420kB kernel_stack:4448kB pagetables:1984kB unstable:0kB bounce:0kB free_pcp:108kB local_pcp:72kB free_cma:103800kB writeback_tmp:0kB pages_scanned:2168 all_unreclaimable? yes
[ 160.686537] lowmem_reserve[]: 0 0 188 188
[ 160.686569] HighMem free:150368kB min:188kB low:664kB high:1144kB active_anon:59144kB inactive_anon:4152kB active_file:8032kB inactive_file:31552kB unevictable:0kB isolated(anon):0kB isolated(file):0kB present:258048kB managed:258048kB mlocked:0kB dirty:0kB writeback:0kB mapped:30452kB shmem:4328kB slab_reclaimable:0kB slab_unreclaimable:0kB kernel_stack:0kB pagetables:2880kB unstable:0kB bounce:0kB free_pcp:120kB local_pcp:12kB free_cma:63996kB writeback_tmp:0kB pages_scanned:0 all_unreclaimable? no
[ 160.686575] lowmem_reserve[]: 0 0 0 0
[ 160.686594] DMA: 185*4kB (UMC) 97*8kB (UM) 2*16kB (U) 3*32kB (C) 6*64kB (C) 3*128kB (C) 0*256kB 3*512kB (C) 1*1024kB (C) 1*2048kB (C) 24*4096kB (C) = 105324kB
[ 160.686664] HighMem: 4*4kB (UC) 4*8kB (UMC) 13*16kB (UMC) 5*32kB (UMC) 37*64kB (UMC) 29*128kB (MC) 6*256kB (MC) 4*512kB (UMC) 1*1024kB (C) 2*2048kB (C) 33*4096kB (MC) = 150368kB
[ 160.686739] 11627 total pagecache pages
[ 160.686746] 0 pages in swap cache
[ 160.686753] Swap cache stats: add 0, delete 0, find 0/0
[ 160.686759] Free swap = 0kB
[ 160.686764] Total swap = 0kB
[ 160.686770] 252928 pages RAM
[ 160.686776] 64512 pages HighMem/MovableOnly
[ 160.686781] 102916 pages reserved
[ 160.686786] 61440 pages cma reserved

scenario details:
1.process name: zadas_ui, for rendering widget in different mode. 
2. enable diff modes sequentially by click.
3.if loading increases, The process oom, and file-rss value: 140M, but mem has more than 200M left
 
when app widgets first create, following egl aps will be invoked,  glGenTextures-> glBindTexture -> glTexImage2D->glDrawArrays
for widgets texture will not be destoryde for the app whole  lifecycle.
 
our zadas_ui app in user space will ask for allocation to render Texture. As attached log in (https://e2e.ti.com/support/processors/f/791/t/971834?tisearch=e2e-quicksearch&keymatch=oom), there are so much page allocated error logs, when egl create fence sync error occurred. does the remaining mem which mapping to V ram is lower than threshold?
 
and we try echo 1 >> drop_caches , oom still happened
 
this is omm-meminfo log oom_meminfo.xlsx

 

  • Hello,

    Sorry for the delayed follow up. Are you still using this issue?

    We seem to be clearly running out of memory (failure in alloc_pages). Please note that the GPU cannot use memory in highmem.

    Does this happen over a period of time? Have you looked to see if available memory decreases? Wondering if there is a leak in system.

    Regards

    Hemant