Other Parts Discussed in Thread: XIO2213A, TMDSEVM572X, XIO2213B
Hi Folks,
I am trying to bring up a TI XIO2213A 1394B interface via the PCIe slot on the EVM. I am using TI's XIO2213ZAY reference board for the FireWire card.
I have rebuilt the kernel using the Linux PSP included in the ti-ezsdk_c6a816x-evm_5_00_00_56 (e.g. /psp/linux-2.6.34-psp04.00.00.07) and enabled the new FireWire stack.
The OHCI controller is recognized on the PCIe bus and the driver is loaded.
If I connect a FW HD to the Firewire bus, the device is recognized, the SBP-2 driver is loaded and the FAT filesystem on the drive is mounted.
If I then do a ls on the filesystem, I get a kernel panic:
root@c6a816x-evm:~# ls /media/sda1/
Unhandled fault: Precise External Abort on non-linefetch (0x1008) at 0xca87a080
Internal error: : 1008 [#1]
last sysfs file: /sys/kernel/uevent_seqnum
Modules linked in: bufferclass_ti omaplfb pvrsrvkm TI81xx_hdmi(P) ti81xxfb vpss syslink ipv6
CPU: 0 Tainted: P (2.6.34 #1)
PC is at at_context_transmit+0x460/0x510
LR is at ___dma_single_cpu_to_dev+0x60/0x70
pc : [<c0200ae8>] lr : [<c00379d0>] psr: 60000093
sp : c6bb59e0 ip : c6bb59e0 fp : c6bb5a54
r10: c7011000 r9 : 00000093 r8 : c7011000
r7 : c7011534 r6 : c6ad1014 r5 : ffc61d60 r4 : c6ad106c
r3 : ca87a000 r2 : 00000003 r1 : 86ad106c r0 : 00000003
Flags: nZCv IRQs off FIQs on Mode SVC_32 ISA ARM Segment user
Control: 10c5387d Table: 8682c019 DAC: 00000015
Process ls (pid: 1233, stack limit = 0xc6bb42e8)
The PC where the exception occurs is a register access in the Firewire-OHCI driver drivers/firewire/ohci.c line 1036:
reg_read(ohci, OHCI1394_IntEventSet) & OHCI1394_busReset) {