Do all the Component video pins can be used for TV output pin?
The apps requires 4 standard TV outputs from DSP chip, I am wondering if those component video pins can be re-configured to be used for other TV out?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Do all the Component video pins can be used for TV output pin?
The apps requires 4 standard TV outputs from DSP chip, I am wondering if those component video pins can be re-configured to be used for other TV out?
jim xu,
Which ti dsp chip you are referring to? Are you referring to pin configuration in any document? Please provide more details.
I referred the DM368. There are 3 TV_Out pins, and 3 component video pins in document. Do those component pins can be configured ?
Basically, what I need is processing 4 channel of video from pixel based input into PAL/NTSC output (D1), if I use DM368, what other IC do I need to accomplish the task?
Thanks.
No, unfortunately the 3 DACs cannot be re-configured for 3 independent CVBS signals.
BR,
Steve
As you suggested in another thread, I better use separated FPGA to do 4 channel, forget about the TV_Out, right?