This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[TDA4M] How to create bootable sdcard in linux for J721E SBL

Hi,

Can I get some guide to make a bootable sdcard for J721E EVM?

I used a PSDK ver7.1 and I've checked the user guild in Bootloader(SBL)/J721E SBL/Boot Modes/Booting Via SD Card.

In there, 

Preparing the SD card

  1. To boot the target the SD card should be bootable. Follow the steps at Creating bootable SD card in windows or Creating bootable SD card in Linux.
  2. To update the SBL with a newer version, copy the sbl image (sbl_mmcsd_img_mcu1_0_release.tiimage) to the SD card. Rename it to tiboot3.bin
  3. Copy the generated application image(*.appimage or *.appimage.signed) to the SD card. Rename it to app

Click 'Creating bootable SD card in Linux, then this link is opened.

1.1. Processor SDK RTOS Getting Started Guide — Processor SDK RTOS Documentation

But, I can't find the create-sdcard.sh file. 

Best regards

Yongsig.