Part Number: TMDSICE3359
Other Parts Discussed in Thread: PROFIBUS,
Hi,
I'd like to use UART1 without PRU as RS485 port and I think that I could activate pin D17 LATCH1_IN to UART1_RTS but I have to solder the line to DE pin of the Profibus transceiver because there is no UART1_RTS in pin C13 (GPIO3_19). But what should I do to make this pin change to work in Yocto build? My Yocto workspace is based on software-dl.ti.com/.../Overview_Building_the_SDK.html and I build it as MACHINE=am335x-evm bitbake arago-base-tisdk-image.
Regards,
Jani