Part Number: TDA2EG-17
Dear TI team:
Does the cpts module support capturing external PPS signals for synchronization or clock calibration?
Application background:1.Customers need to support the gPTP function on the board.Our board is used as masterclock, but it needs to be aligned with PPS and GPRMC sentence。
And our board has a GNSS receiver that can provide PPS signals.
2.I use the open source project Linuxptp to meet this function,and ts2phc is a subroutine in linuxptp to align the PHC clock to the PPS .But the driver /dev/ptp0 does not support
Doubt:
I see that keystone2 supports direct triggering of the hardware pps pin. Is there a big difference between these twochips?
downloads.ti.com/.../Foundational_Components_Kernel_Drivers.html
And if the cpts module support capturing external PPS signals ?