I want to design a PDA have 2 camera ,1 in front (to video diague) ,1 in behind---(to take a photograph) ,can I achieve this design. The video dialogue is used in the facture inside employees ,can the 1GHz AM3715 can process this task .The video diague and Wireless Communications are basic on the WIFI .
Who can tell me how to connect the 2 camera sensors into the AM3715?
Who can tell me the 1 bit ECC flash Reference Design‘s type and part number to design AM3715 PCB .
If use the AM3715 to do Video processing , what Highest Capacity AM3715 can do?