Other Parts Discussed in Thread: TCI6638K2K
Hi,
I am working on a project that uses Makefile on TCI6638K2K board. Until now, we compiled the project on Windows with GNU GCC 7.2.1 compiler. We downloaded the compiler from "developer.arm.com/.../downloads". We are using "gcc-arm-none-eabi-7-2017-q4-major-win32.exe". That is the 32bit version of GCC.
For testing on Linux, we compiled the project using Ubuntu 20.04 GNU GCC 7.2.1. We downloaded the compiler from "developer.arm.com/.../downloads". We are using "gcc-arm-none-eabi-7-2017-q4-major-linux.tar.bz2". That is a 64bit version of GCC (32bit version of GCC for Linux is not available on that website).
Somehow, the outputs of Linux is not performing the same performance as the outputs of Windows.
There are some differences between Linux and Windows outputs. For example; while Windows aligns sections to 4byte, Linux aligns to 8 bytes; while Windows maps functions&variables to 32bit addresses, Linux maps functions&variables to 64bit addresses.
Could the difference in the alignment&mapping, cause the above-mentioned performance inequality?
Is there any way to use "gcc-arm-none-eabi-7-2017-q4-major-linux.tar.bz2" and create outputs as 32bit on Linux?
Thank you, Best Regards,