This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3356: Uart baud rate

Part Number: AM3356

Hi,

SDK: ti-processor-sdk-linux-rt-am335x-evm-06.03.00.106

The customer has configured two serial ports in the PRU1 in dts, namely /dev/ttySPRU3 and /dev/ttySPRU4. The output waveform of the serial port output data is normal with an oscilloscope, but the baud rate error is large. The 9600 baud rate actually looks It is about 6K or more. The 4800 baud rate sees more than 3K. But looking at pru_suart.c in the linux driver, there is no interface for setting the pru clock frequency.  The code of the pru firmware has not been modified yet.