Other Parts Discussed in Thread: AM3505, SN75LVDS83
I understand that the AM3505 supports up to 24-bit TFT LCD control with a parallel interface. However, the bigger color LCD's (>10.4" VGA or higher resolution) are now requiring an LVDS control interface. Looking at some of these display's, it appears the LVDS control interface contains 1 differential pair of clock and 4 differential pairs of serial data.
Can any advise if the AM3505 can be used to control these LCD's with an LVDS interface? Or would this require an external LCD controller?