This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: CAN profile application is not working with SPL (with linux)

Part Number: TDA4VM

Hi,

I'm using PSDK 7.1 and I want to run can profiling app with the linux , I don't see any CAN demo which works with Linux environment.

I have build the CAN profile app demo and build the u-boot with DM=path for app and I have updated u-boot.img and tispl.bin and I have done the soft link of the can profile app under /lib/firmware.

In the linux terminal, I 'm getting only below logs. It's not booting u-boot.

==============================================

U-Boot SPL 2020.01-g3c9ebdb87d (Nov 19 2020 - 18:33:21 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0014 '20.8.5--v2020.08b (Terrific Lla')
Trying to boot from MMC2
Loading Environment from MMC... *** Warning - No MMC card found, using default environment

Starting ATF on ARM64 core...

NOTICE:  BL31: v2.3():07.01.00.004-1-g52c334fc3-dirty
NOTI����'H��L31: Built : 18:17:14, Nov 19 2020

==============================================

Can you please give your suggestions ?

Thanks,

Pooja

  • Hi Pooja,

    You can use patch from Karan, which is here /cfs-file/__key/communityserver-discussions-components-files/791/0001_2D00_mcu1_5F00_0_2D00_can_5F00_profile_5F00_app_2D00_make_2D00_changes_2D00_to_2D00_load_2D00_from_2D00_R5_2D00_.zip

    It's basically from sdk7.0 but you compare and apply manually on sdk7.1. It will work.

    Thanks,

    -Makani

  • Thanks for sharing the patches, Amit.

    Hi Pooja,

    Please let us know if this unblocked you or looking for any support.

    Thanks & Regards,

    Sunita.

  • Yes, it resolved my issue

  • Yes, it resolved my issue.

  • Yes, it resolved my issue.

  • Yes, it resolved my issue.

  • Yes, it resolved my issue.

  • I am using PSDKRA 7.1.

    I want to integrate a Cdd Ipc linux RPROC demo application with Can demo application which can run along with linux.

    I verified Cdd ipc and CAN application to run with Linux individually.

    Now I want to merge this two.

    I have merged linker files as below:

    /*----------------------------------------------------------------------------*/
    /* File: linker_r5f_mcu1_0_btcm_sysbios.lds                                        */
    /* Description:			  					      */
    /*    Link command file for J7ES MCU1_0 view				      */
    /*	  TI ARM Compiler version 15.12.3 LTS or later			      */
    /*                                                                            */
    /* (c) Texas Instruments 2018, All rights reserved.                           */
    /*----------------------------------------------------------------------------*/
    /*  History:								      */
    /*    Aug 26th, 2016 Original version .......................... Loc Truong   */
    /*    Aug 01th, 2017 new TCM mem map  .......................... Loc Truong   */
    /*    Nov 07th, 2017 Changes for R5F Init Code.................. Vivek Dhande */
    /*    Sep 17th, 2018 Added DDR sections for IPC................. J. Bergsagel */
    /*    Sep 26th, 2018 Extra mem sections for IPC resource table.. J. Bergsagel */
    /*    Nov 06th, 2018 Correction to TCM addresses for MCU1_0..... J. Bergsagel */
    /*    Nov 07th, 2018 Split up OCMRAM_MCU for split-mode R5Fs.... J. Bergsagel */
    /*    Feb 20th, 2019 Use R5F BTCM memory for boot vectors........J. Bergsagel */
    /*    Apr 23th, 2019 Changes for R5F startup Code............... Vivek Dhande */
    /*----------------------------------------------------------------------------*/
    /* Linker Settings                                                            */
    /* Standard linker options
    --retain="*(.intvecs)"
    --retain="*(.intc_text)"
    --retain="*(.rstvectors)"						      */
    --retain="*(.bootCode)"
    --retain="*(.startupCode)"
    --retain="*(.startupData)"
    
    --retain="*(.mcuCopyVecsToExc)"
    --fill_value=0
    --stack_size=0x2000
    --heap_size=0x1000
    
    -stack  0x2000                              /* SOFTWARE STACK SIZE           */
    -heap   0x2000                              /* HEAP AREA SIZE                */
    
    #define DDR0_ALLOCATED_START 0xA0000000
    
    #define MCU1_0_EXT_DATA_BASE     (DDR0_ALLOCATED_START + 0x00100000)
    #define MCU1_0_R5F_MEM_TEXT_BASE (DDR0_ALLOCATED_START + 0x00200000)
    #define MCU1_0_R5F_MEM_DATA_BASE (DDR0_ALLOCATED_START + 0x00300000)
    #define MCU1_0_DDR_SPACE_BASE    (DDR0_ALLOCATED_START + 0x00400000)
    
    #define MCU1_1_ALLOCATED_START   DDR0_ALLOCATED_START + 0x01000000
    #define MCU1_1_EXT_DATA_BASE     (MCU1_1_ALLOCATED_START + 0x00100000)
    #define MCU1_1_R5F_MEM_TEXT_BASE (MCU1_1_ALLOCATED_START + 0x00200000)
    #define MCU1_1_R5F_MEM_DATA_BASE (MCU1_1_ALLOCATED_START + 0x00300000)
    #define MCU1_1_DDR_SPACE_BASE    (MCU1_1_ALLOCATED_START + 0x00400000)
    
    #define MCU2_0_ALLOCATED_START   DDR0_ALLOCATED_START + 0x02000000
    #define MCU2_0_EXT_DATA_BASE     (MCU2_0_ALLOCATED_START + 0x00100000)
    #define MCU2_0_R5F_MEM_TEXT_BASE (MCU2_0_ALLOCATED_START + 0x00200000)
    #define MCU2_0_R5F_MEM_DATA_BASE (MCU2_0_ALLOCATED_START + 0x00300000)
    #define MCU2_0_DDR_SPACE_BASE    (MCU2_0_ALLOCATED_START + 0x00400000)
    
    #define MCU2_1_ALLOCATED_START   DDR0_ALLOCATED_START + 0x03000000
    #define MCU2_1_EXT_DATA_BASE     (MCU2_1_ALLOCATED_START + 0x00100000)
    #define MCU2_1_R5F_MEM_TEXT_BASE (MCU2_1_ALLOCATED_START + 0x00200000)
    #define MCU2_1_R5F_MEM_DATA_BASE (MCU2_1_ALLOCATED_START + 0x00300000)
    #define MCU2_1_DDR_SPACE_BASE    (MCU2_1_ALLOCATED_START + 0x00400000)
    
    #define ATCM_START 0x00000000
    #define BTCM_START 0x41010000
    
    -e __VECS_ENTRY_POINT
    --retain="*(.ipcCopyVecsToExc)"
    
    --define FILL_PATTERN=0xFEAA55EF
    --define FILL_LENGTH=0x100
    
    /*----------------------------------------------------------------------------*/
    /* Memory Map                                                                 */
    MEMORY
    {
        /* MCU1_R5F_0 local view  */
        MCU_ATCM (RWX)		: origin=ATCM_START	length=0x8000
        /* MCU1_R5F0_TCMB0 (RWIX)	: origin=BTCM_START	length=0x8000 (documented only, to avoid conflict below) */
    
        /* MCU1_R5F_0 SoC view  */
        MCU1_R5F0_ATCM (RWIX)  	: origin=0x41000000 length=0x8000
        MCU1_R5F0_BTCM_VECS (RWIX)  : origin=0x41010000 length=0x0100
        MCU1_R5F0_BTCM (RWIX) 	: origin=0x41010100 length=0x7F00
    
        DDR0_RESERVED    (RWIX)  	: origin=0x80000000 length=0x20000000	  	/* 512MB */
        MCU1_0_IPC_DATA (RWIX)	: origin=DDR0_ALLOCATED_START     length=0x00100000	/*   1MB */
        MCU1_0_EXT_DATA  (RWIX)	: origin=MCU1_0_EXT_DATA_BASE     length=0x00100000	/*   1MB */
        MCU1_0_R5F_MEM_TEXT (RWIX)	: origin=MCU1_0_R5F_MEM_TEXT_BASE length=0x00100000	/*   1MB */
        MCU1_0_R5F_MEM_DATA (RWIX)	: origin=MCU1_0_R5F_MEM_DATA_BASE length=0x00100000	/*   1MB */
        MCU1_0_DDR_SPACE (RWIX)	: origin=MCU1_0_DDR_SPACE_BASE    length=0x00C00000	/*  12MB */
        MCU1_1_IPC_DATA (RWIX)	: origin=MCU1_1_ALLOCATED_START   length=0x00100000	/*   1MB */
        MCU1_1_EXT_DATA  (RWIX)	: origin=MCU1_1_EXT_DATA_BASE     length=0x00100000	/*   1MB */
        MCU1_1_R5F_MEM_TEXT (RWIX)	: origin=MCU1_1_R5F_MEM_TEXT_BASE length=0x00100000	/*   1MB */
        MCU1_1_R5F_MEM_DATA (RWIX)	: origin=MCU1_1_R5F_MEM_DATA_BASE length=0x00100000	/*   1MB */
        MCU1_1_DDR_SPACE (RWIX)	: origin=MCU1_1_DDR_SPACE_BASE    length=0x00C00000	/*  12MB */
        MCU2_0_IPC_DATA (RWIX)	: origin=MCU2_0_ALLOCATED_START   length=0x00100000	/*   1MB */
        MCU2_0_EXT_DATA  (RWIX)	: origin=MCU2_0_EXT_DATA_BASE     length=0x00100000	/*   1MB */
        MCU2_0_R5F_MEM_TEXT (RWIX)	: origin=MCU2_0_R5F_MEM_TEXT_BASE length=0x00100000	/*   1MB */
        MCU2_0_R5F_MEM_DATA (RWIX)	: origin=MCU2_0_R5F_MEM_DATA_BASE length=0x00100000	/*   1MB */
        MCU2_0_DDR_SPACE (RWIX)	: origin=MCU2_0_DDR_SPACE_BASE    length=0x00C00000	/*  12MB */
        MCU2_1_IPC_DATA (RWIX)	: origin=MCU2_1_ALLOCATED_START   length=0x00100000	/*   1MB */
        MCU2_1_EXT_DATA  (RWIX)	: origin=MCU2_1_EXT_DATA_BASE     length=0x00100000	/*   1MB */
        MCU2_1_R5F_MEM_TEXT (RWIX)	: origin=MCU2_1_R5F_MEM_TEXT_BASE length=0x00100000	/*   1MB */
        MCU2_1_R5F_MEM_DATA (RWIX)	: origin=MCU2_1_R5F_MEM_DATA_BASE length=0x00100000	/*   1MB */
        MCU2_1_DDR_SPACE (RWIX)	: origin=MCU2_1_DDR_SPACE_BASE    length=0x00C00000	/*  12MB */
    
        SHARED_DDR_SPACE (RWIX)	: origin=0xAA000000 length=0x01C00000           /*  28MB */
    
       /* VECTORS (X)             : origin=0x41C3C100 length=0x1000
        RESET_VECTORS (X)       : origin=0x41C40000 length=0x100*/
        RESET_VECTORS (X)       : origin=0x41C3D100 length=0x100
        /*MCU1_0_MSRAM            : origin=0x41C40100 length=0x5C000 - 0x100 */
    
        /*OCMC_RAM_BOARD_CFG (RWIX)   : origin=0x41C80000 length=0x2000
        OCMC_RAM_SCISERVER (RWIX)   : origin=0x41C82000 length=0x60000
        RESET_VECTORS (X)           : origin=0x41CE2000 length=0x100
        OCMC_RAM (RWIX)             : origin=0x41CE2100 length=0x1DA00
        OCMC_RAM_X509_HEADER (RWIX) : origin=0x41CFFB00 length=0x500*/
    
    }  /* end of MEMORY */
    
    /*----------------------------------------------------------------------------*/
    /* Section Configuration                                                      */
    
    SECTIONS
    {
        .vecs : {
             *(.vecs)
        } palign(8) > BTCM_START
        .vecs       : {
            __VECS_ENTRY_POINT = .;
        } > MCU1_R5F0_BTCM_VECS
        xdc.meta (COPY): { *(xdc.meta) } > MCU1_R5F0_BTCM
        .init_text  : {
                         boot.*(.text)
                         *(.text:ti_sysbios_family_arm_MPU_*)
                         *(.text:ti_sysbios_family_arm_v7r_Cache_*)
                      }  palign(8) > MCU1_R5F0_BTCM
        .text:xdc_runtime_Startup_reset__I     : {} palign(8) > MCU1_R5F0_BTCM
        .intvecs 	: {} palign(8) 		> MCU1_R5F0_BTCM
        .intc_text 	: {} palign(8) 		> MCU1_R5F0_BTCM
        .rstvectors : {} palign(8)      	> MCU1_R5F0_BTCM
        .bootCode    	: {} palign(8) 		> MCU1_R5F0_BTCM
        .startupCode 	: {} palign(8) 		> MCU1_R5F0_BTCM
        .startupData 	: {} palign(8) 		> MCU1_R5F0_BTCM, type = NOINIT
        .ipcCopyVecsToExc                   : {} palign(8) > MCU1_R5F0_BTCM
        .mcuCopyVecsToExc : {} palign(8) > MCU1_R5F0_BTCM
        .text	: {} palign(8)		> MCU1_0_DDR_SPACE
        .const   	: {} palign(8) 		> MCU1_0_DDR_SPACE
        .cinit   	: {} palign(8) 		> MCU1_0_DDR_SPACE
        .pinit   	: {} palign(8) 		> MCU1_0_DDR_SPACE
        .bss     	: {} align(4)  		> MCU1_0_DDR_SPACE
        .data    	: {} palign(128) 	> MCU1_0_DDR_SPACE
        .data_buffer: {} palign(128) 	> MCU1_0_DDR_SPACE
        .sysmem  	: {} 			> MCU1_0_DDR_SPACE
        .stack	: {} align(4)		> MCU1_0_DDR_SPACE
        ipc_data_buffer (NOINIT) : {} palign(128)	> MCU1_0_DDR_SPACE
        .resource_table : {
            __RESOURCE_TABLE = .;
        } > MCU1_0_EXT_DATA_BASE
    
        .const.devgroup.MCU_WAKEUP    : {} align(4)      > MCU1_0_DDR_SPACE
        .const.devgroup.MAIN          : {} align(4)      > MCU1_0_DDR_SPACE
        .const.devgroup.DMSC_INTERNAL : {} align(4)      > MCU1_0_DDR_SPACE
        .bss.devgroup.MAIN            : {} align(4)      > MCU1_0_DDR_SPACE
        .bss.devgroup.MCU_WAKEUP      : {} align(4)      > MCU1_0_DDR_SPACE
        .bss.devgroup.DMSC_INTERNAL   : {} align(4)      > MCU1_0_DDR_SPACE
        .boardcfg_data                : {} align(4)      > MCU1_0_DDR_SPACE
        .bss.devgroup*                : {} align(4)      > MCU1_0_DDR_SPACE
        .const.devgroup*              : {} align(4)      > MCU1_0_DDR_SPACE
    
    /*    .benchmark_buffer (NOLOAD) {} ALIGN (8) > MCU1_0_DDR_SPACE */
    
        .benchmark_buffer (NOLOAD) {} ALIGN (8) > MCU1_0_DDR_SPACE
    /* Additional sections settings     */
        McalTextSection : fill=FILL_PATTERN, align=4, load > MCU1_0_DDR_SPACE
        {
            .=align(4);
            __linker_spi_text_start = .;
            . += FILL_LENGTH;
            *(SPI_TEXT_SECTION)
            *(SPI_ISR_TEXT_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_spi_text_end = .;
    
            .=align(4);
            __linker_gpt_text_start = .;
            . += FILL_LENGTH;
            *(GPT_TEXT_SECTION)
            *(GPT_ISR_TEXT_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_gpt_text_end = .;
    
            .=align(4);
            __linker_dio_text_start = .;
            . += FILL_LENGTH;
            *(DIO_TEXT_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_dio_text_end = .;
    
            .=align(4);
            __linker_eth_text_start = .;
            . += FILL_LENGTH;
            *(ETH_TEXT_SECTION)
            *(ETH_ISR_TEXT_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_eth_text_end = .;
    
            .=align(4);
            __linker_ethtrcv_text_start = .;
            . += FILL_LENGTH;
            *(ETHTRCV_TEXT_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_ethtrcv_text_end = .;
    
            .=align(4);
            __linker_can_text_start = .;
            . += FILL_LENGTH;
            *(CAN_TEXT_SECTION)
            *(CAN_ISR_TEXT_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_can_text_end = .;
    
            .=align(4);
            __linker_wdg_text_start = .;
            . += FILL_LENGTH;
            *(WDG_TEXT_SECTION)
            *(WDG_ISR_TEXT_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_wdg_text_end = .;
    
            .=align(4);
            __linker_pwm_text_start = .;
            . += FILL_LENGTH;
            *(PWM_TEXT_SECTION)
            *(PWM_ISR_TEXT_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_pwm_text_end = .;
    
            __linker_adc_text_start = .;
            . += FILL_LENGTH;
            *(ADC_TEXT_SECTION)
            *(ADC_ISR_TEXT_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_adc_text_end = .;
    
            .=align(4);
            __linker_cdd_ipc_text_start = .;
            . += FILL_LENGTH;
            *(CDD_IPC_TEXT_SECTION)
            *(CDD_IPC_ISR_TEXT_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_cdd_ipc_text_end = .;
    
        }
        McalConstSection : fill=FILL_PATTERN, align=4, load > MCU1_0_DDR_SPACE
        {
            .=align(4);
            __linker_spi_const_start = .;
            . += FILL_LENGTH;
            *(SPI_CONST_32_SECTION)
            *(SPI_CONFIG_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_spi_const_end = .;
    
            .=align(4);
            __linker_gpt_const_start = .;
            . += FILL_LENGTH;
            *(GPT_CONST_32_SECTION)
            *(GPT_CONFIG_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_gpt_const_end = .;
    
            .=align(4);
            __linker_dio_const_start = .;
            . += FILL_LENGTH;
            *(DIO_CONST_32_SECTION)
            *(DIO_CONST_UNSPECIFIED_SECTION)
            *(DIO_CONFIG_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_dio_const_end = .;
    
            .=align(4);
            __linker_can_const_start = .;
            . += FILL_LENGTH;
            *(CAN_CONST_8_SECTION)
            *(CAN_CONST_32_SECTION)
            *(CAN_CONFIG_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_can_const_end = .;
    
            .=align(4);
            __linker_eth_const_start = .;
            . += FILL_LENGTH;
            *(ETH_CONST_32_SECTION)
            *(ETH_CONFIG_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_eth_const_end = .;
    
            .=align(4);
            __linker_ethtrcv_const_start = .;
            . += FILL_LENGTH;
            *(ETHTRCV_CONST_32_SECTION)
            *(ETHTRCV_CONFIG_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_ethtrcv_const_end = .;
    
            .=align(4);
            __linker_wdg_const_start = .;
            . += FILL_LENGTH;
            *(WDG_CONST_32_SECTION)
            *(WDG_CONFIG_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_wdg_const_end = .;
    
            .=align(4);
            __linker_pwm_const_start = .;
            . += FILL_LENGTH;
            *(PWM_CONST_32_SECTION)
            *(PWM_CONFIG_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_pwm_const_end = .;
    
            .=align(4);
            __linker_adc_const_start = .;
            . += FILL_LENGTH;
            *(ADC_CONST_32_SECTION)
            *(ADC_CONFIG_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_adc_const_end = .;
    
            .=align(4);
            __linker_cdd_ipc_const_start = .;
            . += FILL_LENGTH;
            *(CDD_IPC_CONST_32_SECTION)
            *(CDD_IPC_CONFIG_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_cdd_ipc_const_end = .;
        }
    
        McalInitSection : fill=FILL_PATTERN, align=4, load > MCU1_0_DDR_SPACE
        {
            .=align(4);
            __linker_spi_init_start = .;
            . += FILL_LENGTH;
            *(SPI_DATA_INIT_UNSPECIFIED_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_spi_init_end = .;
    
            .=align(4);
            __linker_gpt_init_start = .;
            . += FILL_LENGTH;
            *(GPT_DATA_INIT_32_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_gpt_init_end = .;
    
            .=align(4);
            __linker_pwm_init_start = .;
            . += FILL_LENGTH;
            *(PWM_DATA_INIT_32_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_pwm_init_end = .;
    
            .=align(4);
            __linker_dio_init_start = .;
            . += FILL_LENGTH;
            *(DIO_DATA_INIT_32_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_dio_init_end = .;
    
            .=align(4);
            __linker_eth_init_start = .;
            . += FILL_LENGTH;
            *(ETH_DATA_INIT_UNSPECIFIED_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_eth_init_end = .;
    
            .=align(4);
            __linker_ethtrcv_init_start = .;
            . += FILL_LENGTH;
            *(ETHTRCV_DATA_INIT_UNSPECIFIED_SECTION)
            *(ETHTRCV_DATA_INIT_32_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_ethtrcv_init_end = .;
    
            .=align(4);
            __linker_can_init_start = .;
            . += FILL_LENGTH;
            *(CAN_DATA_INIT_8_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_can_init_end = .;
    
            .=align(4);
            __linker_wdg_init_start = .;
            . += FILL_LENGTH;
            *(WDG_DATA_INIT_UNSPECIFIED_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_wdg_init_end = .;
    
            .=align(4);
            __linker_adc_init_start = .;
            . += FILL_LENGTH;
            *(ADC_DATA_INIT_UNSPECIFIED_SECTION)
            *(ADC_DATA_INIT_32_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_adc_init_end = .;
    
            .=align(4);
            __linker_cdd_ipc_init_start = .;
            . += FILL_LENGTH;
            *(CDD_IPC_DATA_INIT_UNSPECIFIED_SECTION)
            *(CDD_IPC_DATA_INIT_32_SECTION)
            *(CDD_IPC_DATA_INIT_8_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_cdd_ipc_init_end = .;
        }
        McalNoInitSection : fill=FILL_PATTERN, align=4, load > MCU1_0_DDR_SPACE, type = NOINIT
        {
            .=align(4);
            __linker_spi_no_init_start = .;
            . += FILL_LENGTH;
            *(SPI_DATA_NO_INIT_UNSPECIFIED_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_spi_no_init_end = .;
    
            .=align(4);
            __linker_gpt_no_init_start = .;
            . += FILL_LENGTH;
            *(GPT_DATA_NO_INIT_UNSPECIFIED_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_gpt_no_init_end = .;
    
            .=align(4);
            __linker_dio_no_init_start = .;
            . += FILL_LENGTH;
            *(DIO_DATA_NO_INIT_UNSPECIFIED_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_dio_no_init_end = .;
    
            .=align(4);
            __linker_eth_no_init_start = .;
            . += FILL_LENGTH;
            *(ETH_DATA_NO_INIT_UNSPECIFIED_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_eth_no_init_end = .;
    
            .=align(4);
            __linker_ethtrcv_no_init_start = .;
            . += FILL_LENGTH;
            *(ETHTRCV_DATA_NO_INIT_UNSPECIFIED_SECTION)
            *(ETHTRCV_DATA_NO_INIT_16_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_ethtrcv_no_init_end = .;
    
            .=align(4);
            __linker_can_no_init_start = .;
            . += FILL_LENGTH;
            *(CAN_DATA_NO_INIT_UNSPECIFIED_SECTION)
            *(CAN_DATA_NO_INIT_32_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_can_no_init_end = .;
    
            .=align(4);
            __linker_wdg_no_init_start = .;
            . += FILL_LENGTH;
            *(WDG_DATA_NO_INIT_UNSPECIFIED_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_wdg_no_init_end = .;
    
            .=align(4);
            __linker_pwm_no_init_start = .;
            . += FILL_LENGTH;
            *(PWM_DATA_NO_INIT_UNSPECIFIED_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_pwm_no_init_end = .;
    
            __linker_adc_no_init_start = .;
            . += FILL_LENGTH;
            *(ADC_DATA_NO_INIT_UNSPECIFIED_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_adc_no_init_end = .;
    
            __linker_cdd_ipc_no_init_start = .;
            . += FILL_LENGTH;
            *(CDD_IPC_DATA_NO_INIT_UNSPECIFIED_SECTION)
            *(CDD_IPC_DATA_NO_INIT_8_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_cdd_ipc_no_init_end = .;
    
        }
        /* Example Utility specifics */
        VariablesAlignedNoInitSection : align=8, load > MCU1_0_DDR_SPACE, type = NOINIT
        {
            .=align(8);
            __linker_cdd_ipc_no_init_align_8b_start = .;
            . += FILL_LENGTH;
            *(CDD_IPC_DATA_NO_INIT_8_ALIGN_8B_SECTION)
            .=align(8);
            . += FILL_LENGTH;
            __linker_cdd_ipc_no_init_align_8b_end = .;
        }
        /* Example Utility specifics */
        UtilityNoInitSection : align=4, load > MCU1_0_DDR_SPACE, type = NOINIT
        {
            .=align(4);
            __linker_utility_no_init_start = .;
            . += FILL_LENGTH;
            *(EG_TEST_RESULT_32_SECTION)
            .=align(4);
            . += FILL_LENGTH;
            __linker_utility_no_init_end = .;
        }
        SciClientBoardCfgSection : align=128, load > MCU1_0_DDR_SPACE, type = NOINIT
        {
            .=align(128);:  BL31: v2.3():07.01.00.004-1-g52c334fc3-dirty
    NOTICE:  BL31: Built : 18:17:14, Nov 19 2020
    
    
    
            __linker_boardcfg_data_start = .;
            . += FILL_LENGTH;
            *(.boardcfg_data)
            .=align(128);
            . += FILL_LENGTH;
            __linker_boardcfg_data_end = .;
        }
        /* This section is used for descs and ring mems. It's best to have
         * it in OCMRAM or OCMC_RAM_SCISERVER */
        McalUdmaSection : fill=FILL_PATTERN, align=128, load > MCU1_0_DDR_SPACE
        {
            .=align(128);
            __linker_eth_udma_start = .;
            . += FILL_LENGTH;
            *(ETH_UDMA_SECTION)
            .=align(128);
            . += FILL_LENGTH;
            __linker_eth_udma_end = .;
        }
        McalTxDataSection : fill=FILL_PATTERN, align=128, load > MCU1_0_DDR_SPACE, type = NOINIT
        {
            .=align(128);
            __linker_eth_tx_data_start = .;
            . += FILL_LENGTH;
            *(ETH_TX_DATA_SECTION)
            .=align(128);
            . += FILL_LENGTH;
            __linker_eth_tx_data_end = .;
        }
        McalRxDataSection : fill=FILL_PATTERN, align=128, load > MCU1_0_DDR_SPACE, type = NOINIT
        {
            .=align(128);
            __linker_eth_rx_data_start = .;
            . += FILL_LENGTH;
            *(ETH_RX_DATA_SECTION)
            .=align(128);
            . += FILL_LENGTH;
            __linker_eth_rx_data_end = .;
        }
    
        .tracebuf   : {}	> MCU1_0_EXT_DATA
    
    }  /* end of SECTIONS */
    
    /*----------------------------------------------------------------------------*/
    /* Misc linker settings                                                       */
    
    
    /*-------------------------------- END ---------------------------------------*/

    Please suggest me the changes required..

    Thanks and regards,

    Pooja More

  • Hi Pooja,

    1. I suggest taking memory map from IPC app as these sections are already taken care on Linux side.

    2. You can take the startup code from one of the applications (CAN or IPC CDD) and required logic from both the applications.

    Please let me know if there are any specific questions.

    Thanks & Regards,

    Sunita.

  • Hi Sunita,

    Yes, with cdd ipc linker file, I am able to run application but I am not getting any log on mcu uart once linux boots.

    Thanks and regards,

    Pooja More

  • Hi Pooja,

    In CDD IPC app we are routing the MCU core traces to a trace buffer which can be pulled from Linux / main UART.

    Did you try dumping the remote core traces with below steps:

    after Linux boots

    1. Check the remote core id

    dmsg | grep remotecore

    2. check the remotecoreX corresponding to MCU core you are using

    then 

    cat /sys/kenel/debug/remoteproc/remoteprocX/trace0

    Thanks & Regards,

    Sunita.

  • Hi Sunita,

    Yes, I tried this method  to check logs of mcu sides which are redirected to linux.

    But on linux I didnot get any logs.

    Thanks and regards,

    Pooja More