This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 - Mpeg TS and Mpeg PS stream Decode?



I wonder if it is possible to decode Mpeg TS and Mpeg PS stream on DM365.

 I’ve tested decoding the two streams mentioned above on EVM board and failed.

Does it require any additional works in order to decode the two?

 

  • The standard DVSDK demo does not have transport stream or any other container format(like mp4, avi etc). It only supports elementary stream decode/encode. Hence your Mpeg TS/PS did not get decoded. You may have to write a demultiplexer s/w in ARM and then feed the elemnatry stream to the codec.

    regards

    Yashwant