Other Parts Discussed in Thread: TMS320C5515
About the MMC interface of TMS320C5515 DSP. I'm going to work with Samsung eMMC moviNAND flash via MMC interface. The Samsung eMMC flash is eMMC v4.41 compatable device that supports 4 bit data and 52MHz clock. Can I run TMS320C5515 with 4 bit data of MMC interface at 50MHz clock in fast mode as specified in Table 6-23 paragraph 6.10.2 or it will support only 20MHz clock with 1 bit data?
Thanks in advance
Yaron