Other Parts Discussed in Thread: TMS320DM648
Factory Team,
Please see the request below from Americas Sales and Apps. (Mark Soisson) If you choose to post a response here, I will communicate it to the field requestor. If you prefer to contact the field requestor directly, please indicate so in a post and I will close this request in our tracking system.
Thank you,
Todd Price
Americas Sales Support Line
*****************************************************************************************
AFA/FAE Requestor's Information
Date Opened: 3/4/2011 12:31:06 PM
Company Name: Sensoray
Contact Name: Dean Anderson
Contact Phone: (503) 684-8005
Contact Email: dean@sensoray.com
Address: 7313 SW Tech Center Drive
City and State: Tigard, OR
Postal Code: 97223
Customer's Application
GPN: TMS320DM648
Non GPN:
Application:
app note
Hi, Do you have an app note or example on decoding from a stream for the DM648 (or possible any other DSP)? The decode example in the DVSDK(video_encdec) is ok, but it relies on the input video signal/capture rate to pace the video encoder(analog video output). We are having issues with choppy video output when there is no input video signal involved. Below is our configuration to better illustrate this: H264 stream--->DM648 h264 codec decoder--->DM648 video encoder-->analog video output. The resulting analog video output is very choppy. Do you have any techniques or app notes to resolve this? Best regards, Dean Anderson SW Engineer Sensoray Company Inc. 503-684-8005
Sales support team,
Could someone pls help me locate an app note to satisfy this request?
Regards, Mark