Other Parts Discussed in Thread: OMAPL138
Hi
I want to control the interface speed between OMAPL138 and the external mDDR (MT46H64M16LFBF-5 IT:B TR)
I have checked the init file and learnt that I can control the speed by configuring these registers
; This section can be used to configure the PLL1 and the EMIF3a registers ; for starting the DDR2 interface. ; See PLL1CONFIG section for the format of the PLL1CFG fields. ; |------24|------16|-------8|-------0| ; PLL1CFG0: | PLL1CFG | ; PLL1CFG1: | PLL1CFG | ; DDRPHYC1R: | DDRPHYC1R | ; SDCR: | SDCR | ; SDTIMR: | SDTIMR | ; SDTIMR2: | SDTIMR2 | ; SDRCR: | SDRCR | ; CLK2XSRC: | CLK2XSRC | ;status |= DEVICE_ExternalMemInit(0x000000C5, 0x00134832, 0x264A3209, 0x3C14C722, 0x00000492, 0x00000000); [EMIF3DDR] PLL1CFG0 = 0x18010001 PLL1CFG1 = 0x00000002 DDRPHYC1R = 0x000000C4 SDCR = 0x02034621 SDTIMR = 0x20913249 SDTIMR2 = 0x3A1EC7E1 SDRCR = 0x00000492 CLK2XSRC = 0x00000000
But there is no document that shows how to config them, do you have any suggestion for this case?
Thanks
Ryder