Part Number: TDA2SX
Hello,
We desire to work with streaming application (using UART modem, "ping google.com" is successful). For this purpose we wish to forward port 80 and 554 for the connected ip camera.
Upon trying to run the following, option dport is not recognized
root@dra7xx-evm:~# iptables -t nat -A PREROUTING -p tcp -i ppp0 --dport 8001 -j DNAT --to-destination 192.168.1.200:8080
root@dra7xx-evm:~# iptables v1.8.2 (legacy): unknown option "--dport"
Try `iptables -h' or 'iptables --help' for more information.
Having tried to run the on same on ubuntu host, the command is successful even though the iptables version was 1.4.21
We made several attempts for port forwarding but unsuccessful
Please help on this. Any workaround or known methods to achieve port forwarding are welcome.
Thanks,
Eshwar J