Part Number: AM5728
Hello,
I have purchased AM5728 SoC and already have one AM5728 Evaluation module. There is a requirement to test all the interfaces present on SoC. I ran the tester software, referring to this LINK both through SD card and JTAG Emulator. However, it seems few interfaces are missing from the tester software for evmAM572x.
I have few queries regarding the testing of the SoC interfaces.
1. What shall be the pre-requisite to test all the interfaces present on SoC. For example, is it OK to run the tester software through an emulator without loading any u-boot or kernel filesystem?
2. How to test the PCIe interface ion the SoC, It is not part of tester software, and also, it seems it is not supported for evmAM572x. Is it so?
2. Similarly, how to test the McASP interface on which TLV32x audio codec is connected on the EVM AM5728. As per the Makefile, this interface is not supported for the evmAM572x board?
3. How to test the buses present on SoC. For example - i2c bus, DDR3 memory bus, etc.?
Regards
Sahil Kalra