Part Number: TDA4VM
Hi,
TDA4VM includes 2 MIPI-CSI2 interfaces, it is said TDA4 ISP only process raw data from the primary MIPI-CSI2 interface,
and TDA4 ISP can not handle raw data from the secondary MIPI-CSI2 interface.
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
Hi,
TDA4VM includes 2 MIPI-CSI2 interfaces, it is said TDA4 ISP only process raw data from the primary MIPI-CSI2 interface,
and TDA4 ISP can not handle raw data from the secondary MIPI-CSI2 interface.
Thanks,
Hi,
It can very well support RAW data from second CSI instance also. VISS works in the memory to memory mode, so it can process data for second instance also.
Regards,
Brijesh