Part Number: AM6442
Dear Team,
My customer's main goal is to standardize the embedded system of the project according to SIL 3/4. They want to utilize certified RTOS or Linux OS on our new generation processors. They have encountered our AM6442. They need detailed information on the following questions:
1. Which RTOS (SafeRTOS, GreenHills, etc.) will be provided or is recommended by TI?
2. Which Linux distribution (Debian, Raspbian, Ubuntu, etc.) will be provided?
3. Which safety certifications will Linux/RT Linux/RTOS provided by TI satisfy?
4. Are the port drivers (I/O ports, USB, etc.) provided by TI? If not, is there any IDE to control the ports of the processor?
5. Is IP STACK for EtherNet/EtherCAT communication provided on the product?
Regards,
Renan