This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: driver development for AM5728 video input port?

Part Number: AM5728


Can you provide any summary guidance or documentation on the drivers necessary to interface with a 16-bit YUV422 decoder, connected to one of the AM5728's video ports?

The hardware is a Semtech GS2971A.

Are there any examples of what the sub-device driver should look like / interfaces / examples / documentation?

From below path i have taken driver and gs2971.ko & gs2971.o files created(Related of v4l2 files taken).

https://github.com/HIO-Project/linux-imx6-nano-imx_3.10.17_1.0.1_ga/blob/master/drivers/media/platform/mxc/capture/gs2971.c

In device tree only linux kernel to change enough are in u-boot also require to add anything?

How to read spi slave data from u-boot or kernel(Manufacture ID or Device ID )?

Actually  below command i entered means no driver found is showing

#dmesg | grep vin3a

i will add all dmesg things in below attachment?

Thanking you sir,

Regards,

Ramachandra.