This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: MCASP audio no data on TX

Part Number: AM3358

Hi,

I am interfacing AM3358 with an audio codec. I am having a problem where I am only seeing data on RX, but nothing on TX of MCASP. The audio codec I am using is Si32178 by Silicon Labs. I have it connected as following:

MCASP1_CLKX --> PCLK (Audio Codec)

MCASP1_FSX --> FSYNC (Audio Codec)

MCASP1_AXR0 (TX) --> DRX (Audio Codec)

MCASP1_AXR1 (RX) --> DTX (Audio Codec)

Here is part of my device tree:

voip_audio_pins: pinmux_voip_audio_pins {
                                pinctrl-single,pins = <
                                        AM33XX_IOPAD(0x9a0, PIN_INPUT_PULLDOWN | MUX_MODE3)     /* mcasp0_aclkr.mcasp1_aclkx */
                                        AM33XX_IOPAD(0x9a4, PIN_INPUT_PULLDOWN | MUX_MODE3)     /* mcasp0_fsr.mcasp1_fsx, INPUT */
                                        AM33XX_IOPAD(0x9a8, PIN_OUTPUT_PULLDOWN | MUX_MODE2)    /* mcasp0_axr1.mcasp1_axr0 */
                                        AM33XX_IOPAD(0x9ac, PIN_INPUT_PULLDOWN | MUX_MODE3)     /* mcasp0_ahclkr.mcasp1_axr1 */

                                >;
                        };


&mcasp1 {
        #sound-dai-cells = <0>;
        pinctrl-names = "default";
        pinctrl-0 = <&voip_audio_pins>;
        status = "okay";
        op-mode = <0>;  /* MCASP_IIS_MODE */
        tdm-slots = <8>;
        num-serializer = <4>;
        serial-dir = <  /* 0: INACTIVE, 1: TX, 2: RX */
                        1 2 0 0
                >;
        tx-num-evt = <8>;
        rx-num-evt = <8>;
                };

I am seeing data on MCASP1_AXR1 (RX) --> DTX , but I don't see anything on MCASP1_AXR0 (TX) --> DRX (Audio Codec) even when audio input is coming.

What could be going wrong here?