Other Parts Discussed in Thread: DA8XX
Hi all,
I am using the OMAPL137 EVM board and i am trying to glow the leds DS1 to DS4, which are connected to GPIO's.
I wrote the program in which i am taking care for configuring the PINMUX to GPIO's, and i am setting the direction and then making the GPIO pin high and low.
But the LED doesn't glow at all, i was suspecting a problem with the PINMUX...
So, when i tried the DEVMEM command to change the value of PINMUX and GPIO, i was unable to see the changes i made to PINMUX.....
I am using kernel version 2.6.32-rc6...
If some one can help me out, like is the problem and how to correct it......
Thanks,
Lokesh