This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: R5 SPL does not load EthFw j7-main-r5f0_0-fw binary after updating to PSDK 7.2

Part Number: TDA4VM

Hello TI,

for some reason after updating to PSDK RTOS 7.2 (for EthFw) and to PSDK Linux 7.2 (for U-Boot) - R5 SPL does not load j7-main-r5f0_0-fw binary present in /lib/firmware on the SD card, as it used to be loaded on PSDK 7.0.

Example of log from PSDK 7.0:

Loading Environment from MMC... *** Warning - No MMC card found, using default environment

Remoteproc 2 started successfully
** File not found /lib/firmware/j7-mcu-r5f0_0-fw **
Starting ATF on ARM64 core...Code

Now before "Starting ATF on ARM64 core..." there are no remoteproc logs and I can confirm that nothing is loaded on the core, since Lauterbach debugger is exiting immediately with "Bus error" message.

I tried the steps described in https://e2e.ti.com/support/processors/f/processors-forum/915474/faq-tda4vm-different-ways-to-load-an-rtos-or-baremetal-application-along-with-linux  in the "Loading from u-boot" section, but it did not change anything.

Regards,

Piotr