This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: EMIF Tool Entry for Twin-die DDR3 Device

Part Number: AM5728


Hi,

We are using 4X Micron  MT41K512M16VRP-107 twin-die SDRAM devices on our design based on AM5728 (each EMIF connected to 2 memory devices), for a total capacity of 4GB. The device configuration is 64 Meg x 8 x 8 banks x 2 die.

- What value should be filled for "Total number of banks" under section 1B of EMIF Tool- 8 or 16?

- Under Step 2- DDR Timings: Should the "Final Datasheet Value" match with the values specified in DDR datasheet?

- 32 data bits are used from the SoC: in this case Col9 has to be included in Step3- Address Mapping. Please confirm. The cell is highlighted in white, not green.

Regards,

Thariq