Part Number: EVMK2G
Other Parts Discussed in Thread: 66AK2G02
Hi, i'm using 66AK2G02 (K2G) Evaluation Module. And i will setting McBSP interface to receive data from same ADC.
- First step configure McBSP pins
mcbsp_pins: pinmux_mcbsp_pins {
pinctrl-single,pins = <
K2G_CORE_IOPAD(0x135c) (BUFFER_CLASS_B | PIN_PULLDOWN | MUX_MODE2) /* PR1_PRU1_GPO14.MCBSP_CLKR */
K2G_CORE_IOPAD(0x1354) (BUFFER_CLASS_B | PIN_PULLDOWN | MUX_MODE2) /* PR1_PRU1_GPO12.MCBSP_CLKX */
K2G_CORE_IOPAD(0x1348) (BUFFER_CLASS_B | PIN_PULLDOWN | MUX_MODE2) /* PR1_PRU1_GPO9.MCBSP_DR */
K2G_CORE_IOPAD(0x1358) (BUFFER_CLASS_B | PIN_PULLDOWN | MUX_MODE2) /* PR1_PRU1_GPO13.MCBSP_FSR */
>;
};
2. i want to use McBSP in frame sync mode. How to configure McBSP in this mode? and which driver should i specify
&mcbsp {
pinctrl-names = "default";
pinctrl-0 = <&mcbsp_pins>;
compatible = "ti,???";
????
status = "okay";
????
};