Other Parts Discussed in Thread: TLV320AIC3101
Hi,
We have custom design with DM365 processor and we have used codec tlv320aic3101 In hardware, there is only one input available which is MIC2R/LINE2R. Rest of the inputs are grounded.
We are using board-dm365-evm.c as our reference. and we are also using the kernel from arago git 2.6.32-rc2-davinci1
I used the arecord utility to record
the audio but it hangs and does not record any audio.
Here is the kernel log for the device
###################################################
No device for DAI tlv320aic3x
No device for DAI davinci-i2s
asoc: tlvaic3x <-> davici-i2s mapping ok
ALSA device list:
#0: DaVinci EVM (tlv320aic3x)
###################################################
Please help me with this issue.
Thanks and Regards,
Jagdish