This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can dvsdk3.x support DM6446?

I installed dvsdk3.10, set DEVICE=dm6446 in xdcpath file, it cannot  go through the build when building all_codecs...

but when set DEVICE=dm6467,  it builds well.    So I doubt if dvsdk3.x can support DM6446.. 

Or Some one can help me to support DM6446 with dvsdk3.x